Skip to content

2026

Active Exploitation of CVE-2026-110936 in Siemens Software Center

Siemens has validated that there is an active exploitation of CVE-2026-110936, a DLL side-loading vulnerability in Siemens Software Center. Siemens fixed the weakness in version 4.0.9.8 and published advisory SSA-580366 on 15 October. Existing installations update automatically the next time they start.

No Siemens system, product or update channel was breached to our knowledge. EDR vendors and authorities have been engaged for intelligence sharing, enabling broader detection coverage and coordinated defensive actions.

Increasing Vulnerability Transparency with Supplier-ADP

Since 2024, the Cybersecurity and Infrastructure Security Agency (CISA) has implemented the “Vulnrichment” program to enrich CVE data with additional information. The goal is to give additional context and help defenders in assessing the specific risk of these vulnerabilities. Each CVE from cve.org or github has an Authorized Data Publisher (ADP) container where this data is stored.

As a next level, Siemens PSIRT was advocating a further extension of this: The Supplier-ADP (SADP), which was piloted in the last months and finally introduced in April 2026. The SADP comes handy if a supplier like Siemens wants to add information to a vulnerability, which originates in an upstream dependency.