Java4Shell - Vulnerability in OpenJDK Java (CVE-2026-114938)

Siemens is aware of a remote code execution vulnerability, CVE-2026-114938, referred to as Java4Shell, in OpenJDK. It results from an out-of-bounds write in the optimized Base64 decoder of the OpenJDK HotSpot JIT compiler on x86-64 processors with AVX-512 VBMI support, where malformed Base64 input can corrupt heap memory, allowing disclosure of memory contents or remote code execution.

We are evaluating the impact to Siemens products. For Siemens products that are affected by CVE-2026-114938, corresponding security advisories (SSA) will be published as soon as the related information becomes available.

OpenJDK versions 17 (from 17.0.6), 21, 25 and 27 are affected, up to and including 17.0.21.0.3, 21.0.13.0.3, 25.0.5.0.3 and 27.0.1.0.3. Fixes are available, for example in JDK 17.0.21.1. Further information is available in the following sources:

Note: Please be aware that links in the Blog Post may refer to external websites and content.